DMU Tab missing on File New

2024-03-04T12:20:50Z

Summary


Details

The DMU tab no longer appears on the File New dialog in managed NX2212.


Platforms
  • INTL64 windows-10_1809
Release Versions
  • NX V2212
Solution

This was an intentional change in NX2212 and is "as designed".

In NX2212, there must be a Design displayed for an assembly before the ability to create "New DMU Workset" is available in the NX session. The DMU template selection tab is presented at that time in the Create Workset dialog.

In NX2212, users now have to open (or create) a file. Then in the menu ribbon go to the 'Assemblies' tab and select the 'New DMU Workset' icon to display the DMU templates.


Notes

KB Article ID# PL8736460

Contents

SummaryDetails

Associated Components