In this scenario, a user sees unusual behavior, where the buttons in the Solid Edge Engineering Reference dialog interface display unreadable captions.
This problem may be caused by a new font installation, and removing the font can solve the issue.
When a new font is installed on the computer, it can cause conflicts with the existing fonts, which may result in unexpected behavior in some applications, as seen above with the unreadable captions. This can happen when the font is not installed correctly or is incompatible with the system.
Check if a new font was installed to the system and remove it by accessing the font settings in the operating system and uninstalling the font in question.
Once the font is removed, restart the computer to ensure that the changes take effect.
If the new font installation was the cause, the problem with the illegible Engineering Reference interface display should now be gone.
Notes