Visualization Preferences related to Smooth Edges are lost

2023-09-14T01:43:27Z

Summary


Details

After changing various settings related to "Smooth Edge" from "Visualization Preferences" in Modeling environment, moving to Pre/Post environment and getting back to Modeling, the preferences return to the initial values.

Reproduced Steps:

1. In Modeling, File > Preferences > Visualization...

2. Rendering node > Smooth Edges

3. e.g., change the value of Line Style, Line Width and Angle Tolerance


4. Move to Pre/Post environment

5. Get back to Modeling

6. Confirm the preferences with performing Step1 and Step2

Solution

The behavior is due to NX problem and has been fixed in NX 2306 Series.

Workaround:

There is no effective workaround, and there is no other way than to re-set it in Modeling environment.

Notes

Conditions for problem occurrence

- NX Series: NX 1926 and higher

- Environment : Switching the environment to Pre/Post, Motion or Design from Modeling


- Preferences : Visualization Preferences > Rendering node> Smooth Edges and Style

***Please refer to PL8736204 for Japanese article.

Release Versions
  • NX V2015
  • NX - SYSENG V2015
Platforms
  • Windows x64 10

KB Article ID# PL8736205

Contents

SummaryDetails

Associated Components