Can the Solid Edge Context Toolbar be customized?

2023-09-01T14:00:16Z

Summary


Details

A customer has inquired about the possibility of customizing the Solid Edge Context Toolbar to suit their users individual needs.  They ask if it is possible to add or remove certain commands from the toolbar.

Assembly Context Toolbar example

Solution

The Solid Edge Context Toolbar is designed to show a fixed set of commands that cannot be edited by the user.  The commands displayed on the toolbar are the most commonly used commands in each Solid Edge Application e.g. Assembly for the selected elements, either from the Pathfinder or from the graphics area.

The commands on the Context Toolbar have been added based on data obtained by Development, which has enabled them to identify the most frequently used commands and add them to the toolbar.

Currently there is no way to customize the Context Toolbar by adding or removing commands.

Notes

Note: While the Solid Edge Context Toolbar is not customizable, the Quick Access Toolbar can be customized to suit individual preferences.  This provides users with a way to personalize their experience and add frequently used commands to the toolbar.

KB Article ID# PL8735508

Contents

SummaryDetails

Associated Components