Unable to export assembly to STEP containing parts with different units

2023-08-24T01:28:53Z

Summary


Details

After exporting an assembly with multiple unit systems such as MM and Inch to a STEP file and loading (importing) it in the viewer or CAD, the geometries do not exist. No problem for standalone NX, but a problem for Teamcenter integration.

Reproduced Steps:

1. Start NX from Teamcenter portal

2. Create some parts with Multiple Unit Systems in Assembly

3. File > Export > STEP214

 - File tab > select File System as Output File Destination

 - Data to Export tab > select Selected Objects as Export > select all the objects in Graphic > OK


4. The result of opening the exported STEP in NX


Solution

This behavior is due to NX problem and has been fixed in NX 2212.

Workaround:

Make use of “Enter Part” as “Export”

Notes

This issue only occurs in NX 2206 Series, and only occurs with Teamcenter integration.

It occurs in all STEP translator formats (AP203, AP214, AP242).

Refer to What's new in NX 1980 (Support for exporting mixed unit objects):

https://docs.sw.siemens.com/en-US/doc/209349590/PL20200522120320484.whatsnew/xid1972381

***Please refer to PL8735403 for Japanese article.

Release Versions
  • NX V2206
  • NX - DESIGN V2206
Platforms

    KB Article ID# PL8735404

    Contents

    SummaryDetails

    Associated Components