NX Performing Save As in NX Diagramming

2023-08-24T14:26:01Z
NX for Design

Summary


Details

In the NX Diagramming application there is no Save As command available when running with Teamcenter. Only Save and New. The Save As option is available when running NX Diagramming without Teamcenter (native).

How do I save a Diagramming sheet to a new item when running with Teamcenter?

Solution

The NX Diagramming application uses Intelligent Save Management to control how diagramming objects are saved. This means all save operations are completed using File > Save and then the use can select whether to Save as or Revise the object.

The configuration of the Save Management for Diagramming is described in the help documentation here:

https://docs.sw.siemens.com/en-US/doc/209349590/PL20221117716122093.diagramming/xid2139197

Once this has been configured as required the Save operation on a diagramming object (e.g. Sheet) will provide options for the Save Action as shown below:


KB Article ID# PL8735321

Contents

SummaryDetails

Associated Components

Diagramming Teamcenter Integration for NX