How to hide all wires in an assembly

2024-01-17T12:00:17Z

Summary


Details

In this scenario, the user wants to hide all subassembly wires within their Solid Edge top level assembly, then create a configuration and use that in an subsequent draft. 

Solution

This is a fairly simple thing to do.

First, create a Query to look for wires.



Make sure that the top node assembly is selected. Everything will be selected as shown above.

Run the query.

The wires will be selected.


Uncheck "Show".  The wires will be hidden.

The image below shows the "before" state - the wires are to the right.


The image below is after the wires are hidden. 


The query can be expanded to include Harnesses also.

KB Article ID# PL8735215

Contents

SummaryDetails

Associated Components