NX Ray Traced Studio image has Pink / Magenta Colouring in NX2306

2023-08-15T13:16:41Z
NX for Design

Summary


Details

When creating a Ray Traced Studio (RTS) Image the colours are changed to Pink or Magenta and the image does not match the NX display. 

For Example: 


Solution

This issue has been fixed by PR 10772266 in NX 2306.4000 - August 2023 Monthly Update.
In earlier versions of the NX2306 series the issue can be corrected by copying the file dbgHelp.dll from C:\Windows\System32 to the NXBIN folder in the NX installation. For example, C:\Program Files\Siemens\NX2306\NXBIN

Please note, this .DLL file can only be copied from the same machine, it is non-distributable so cannot be copied to or from other machines. Always create a backup of the original dbgHelp.dll in the NXBIN folder in case this needs to be reinstated.

KB Article ID# PL8734837

Contents

SummaryDetails

Associated Components

4th Generation Design Assemblies CAD Translators Diagramming Drafting FloEFD Industrial Electrical Design Line Designer Mechatronics Concept Designer Modeling NX Legacy Documentation PCB Design PMI Routing Sheet Metal Ship Design Structure Designer Teamcenter Integration for NX Tooling Design Topology Optimization for Designers