Tecnomatix On simulation drivedevice (custom xml command) is ignored

2023-08-28T13:26:05Z
Process Simulate

Summary


Details

On simulation drivedevice (custom xml command) is ignored.

Example:

# Destination My clamp A10

# Drive OPEN

Platforms
  • na windows-1064
Release Versions
  • Tecnomatix V16.1
Solution

- Check the simulation monitor for errors/warnings.

- It could be File / Options / Ignore Logic.

- Object names with space can be problematic since space is the separator for # commands (especially the ones with multiple arguments). This was the cause in this case (shown in problem example).

Working fine example would be as ahead, where the object was renamed, and spaces were replaced by underscores:

# Destination My_clamp_A10

# Drive OPEN

Notes

KB Article ID# PL8733953

Contents

SummaryDetails

Associated Components

Process Simulate Off-Line Programming (OLP)