Repairing Parts and Assemblies in NX - Part 2

2023-08-14T21:19:18Z

Summary


Details

Parametric Features out of date

Solution

Users can manually prevent Parametric Features from automatically updating within a single part file (see image 4). While the option immediately below allows users to Update Model, using Feature Replay allows a user to both update the model and identify if there are any problems with one or more features within the single part file.

Using Make First Feature Current will suppress all Parametric Features within a single Part File and then selecting Play will rebuild them which will ensure all features are up to date. The update will stop on each feature that cannot match all of its original creation settings, so if there is a missing face, edge, etc. This allows users to identify and manually resolve any features with problems or delete them if no longer needed.

To run this function:

'Home (tab) -> Edit Feature (group) -> Feature Replay -> Make First Feature Current (see Image 1) -> Feature Replay (see Image 2) -> Play (see Image 3)'.

Image 1


Image 2


Image 3


Image 4


KB Article ID# PL8733451

Contents

SummaryDetails

Associated Components