Solid Edge 2023 Update 0007 Announcement

2023-08-07T15:26:50Z

Summary


Details

August 7, 2023

Dear Solid Edge Customer:

Solid Edge 2023 Update 0007 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2023 Update 0007

Version: 2210.0007.005 x64

Download Solid Edge 2023 (v2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10665604: Some parts do not display correctly in the Assembly

PR 10691289: Solid Edge crashed while opening an Assembly

PR 10691588: Assembly relations got corrupted when opening an Assembly

PR 10720344: Solid Edge crashed when starting a sketch in part after placing a subassembly

PR 10453306: Fastener system bolt selection shows all lengths of screws after placing the system once

PR 10666537: Error with assembly features - not all holes/cuts created

PR 10733307: Solid Edge crashed while redefining an existing point in the context of an internal component

PR 10216716: Problem accessing a parent object of a Line3D from the Tube object

PR 10646917: Reset Item Numbers does not work properly

PR 10735560: Rotating this assembly is very slow in Update 5

PR 10759958: It is not possible to thread an existing hole in an Assembly

PR 10763546: Replace face after placing a round crashed Solid Edge

PR 10543375: Cannot switch to the design assembly

PR 10748215: Solid Edge crashed when opening this assembly

PR 10778644: Solid Edge crashed when changing the adjustable part length

PR 10783242: Decal disappears when reopening the file in the same session

PR 10751792: A 3D view is missing from the HTML output

PR 231670: Fixed a problem locating items in Pathfinder after scrolling

===Draft===

PR 10740562: Crash when transferring hole table origins onto a layer in draft

PR 10679175: Mass (Quantity) wrong for Sub-Subassemblies

PR 10766835: Deleting a centerline crashes Solid Edge

PR 8686186: Cannot escape from Smart Dimension when in the context menu

===General===

PR 10759199: Pathfinder returns to the main window when clicking

PR 10758367: KeyShot is opened in Demo Mode when using Siemens Mechanical Design2

===Part/Profile/Sheetmetal===

PR 10730596: Solid Edge crashed when creating a sketch

PR 10736498: "Blank" (Flat) works on one part but not the other in almost identical parts

PR 10752521: Solid Edge crashed after using Publish 3D PDF with new 3D PDF Template

PR 10716925: Chamfer with two surfaces: dimensions not displayed when editing dynamic

PR 10734748: 3D-Sketch dismantled after using Lock relationship

PR 10780974: Vertical Command Bar selection filter is not given automatic focus

PR 10685866: Unable to use hotkeys for key point location of Steering Wheel

PR 10724163: Cannot change feature name inside move face feature

PR 10741560: Thin wall caused Solid Edge to crash

PR 10764678: High GPU memory usage, impacting Solid Edge performance

PR 10780419: Solid Edge crashed when creating a Sketch before finishing a Delete face

PR 10785527: Flat pattern - flange missing after flattening

PR 8682520: Solid Edge crashed during the tangency setting for a 3D curve

PR 8682650: No tangent relation for a 3D curve in ordered mode

===SEDM===

PR 10738589: Incorrect file name with "Rename" command

PR 10738831: Find duplicates replacement file needs to be selected manually

PR 10729392: Unable to change Status to Release of a part that has a status of "In Review"

===SEEC===

PR 10744869: 3D Compare failed to create a graphic preview in SEEC

PR 10392270: PDF file not aligned with draft after canceling save

PR 10485398: Item without 3D (VC) does not update in SEEC after removing an occurrence

PR 10666187: When FOA members are published, you cannot select specific members to save

PR 10741147: Occ_Id property on relation Machine

PR 10757738: SEEC_WorkFlow_PDF_Generation.exe adds "tt" to custom property

PR 10704704: Solid Edge assembly synchronization disabled while opening assembly

PR 10666306: Doubled qty in Structure Manager

PR 10780435: Multi-Cad is unable to reload foreign data when no SE dataset is used

===Translators===

PR 10747600: Need to Open NX 2306 Files in Solid Edge 2023 and 2024

PR 10761106: Vent Command Error Dialog

PR 10726267: When translating daft to DWG, a leader line of Callout is broken

PR 10772186: Solid Edge file is not exported in .3mf format for this workflow

PR 10747957: Solid Edge crashed during Compare Model

PR 9991850: Inventor Data Migration fails

KB Article ID# PL8733396

Contents

SummaryDetails

Associated Components