Solid Edge Unable to move dimensions of imported DWG

2023-08-08T15:30:45Z
DRAFT

Summary


Details

In this example, the user imports a DWG into a Solid Edge Draft file.  They subsequently find that it is not possible to move the dimensions attached to the view.


The result is that only the curves and lines will be moved, whilst the dimensions will not be moved.


Solution

The workaround to this is to "Show" the hidden translation layer in the Layers window.


Now it will be possible for the dimensions to be moved.


KB Article ID# PL8733035

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS