User expressions are created in sheet metal settings

2023-08-07T04:12:56Z

Summary


Details

The expressions that should have been created as a global expression by Sheet Metal setting is automatically created as the user expressions. As the result, is listed in the user expression field.

Reproduced Steps:

1. Model tab in File New > select Sheet Metal template > OK

2. File > Preferences > Sheet Metal > OK( with keep the default)


3. Confirm the created expressions in Part Navigator( Automatically the user expressions will be created.)


Solution

The behavior is due to NX problem, has been fixed in NX 2206 Series so that the global expressions are not generated as the user expressions.

Notes

The behavior occurs in NX 1980 and NX 2007 Series.

The system does not refer to the user expression on the part navigator but refers to the set values stored internally, so there is no effect even if the values are changed by mistake from the part navigator.

***Please refer to PL8732979 for Japanese article.

Release Versions
  • NX V1980
  • NX - DESIGN V1980
Platforms
  • Windows x64 10

KB Article ID# PL8732981

Contents

SummaryDetails

Associated Components