Where can I find an example of the Data Preparation Utility?

2023-08-14T13:46:36Z

Summary


Details

Data Preparation Utility example.

Platforms
  • INTL64 windows-1064
Release Versions
  • Solid Edge V223.0
Solution

The general steps are;

1. Have a folder where the Solid Edge documents reside.

2. 'Start -> Siemens Solid Edge 2023 -> Choose PDM Integration'.

3. 'Teamcenter -> Utility'

4. Click on 'Select Files/Folders'.

5. Click on 'Add File' for this example.

6. Browse to the folder where the Solid Edge documents are and make the selection (select all for this case). Then click on 'Generate Import List'.

7. Fill the required columns (yellow) and save the spreadsheet and save.

8. Click on 'Modify Properties'. This will inject the filled cell values into the Solid Edge documents.

9. Solid Edge documents are now ready to be uploaded to Teamcenter.

Notes

KB Article ID# PL8732837

Contents

SummaryDetails

Associated Components