Angular dimension unit "°" is not displayed but "S" is displayed

2023-08-02T01:45:40Z

Summary


Details

When using Arial text font and setting the angular dimension display to "Show as Fraction", the unit "°" is not displayed and instead "S" is displayed.

Reproduced Steps:

1. After setting Text Font to “Arial”, create an Angular dimension


2. Select the dimension > Mouse right click > Settings > Text > Units > Show as Fraction


Solution

The behavior is working as expected.

Workaround:

Please use NX Fonts.


Notes

The text font to be supported by “Show as Fraction” is only NX Fonts. Windows Standard font has not been supported.

***Please refer to PL8731647 for Japanese article.

Release Versions
  • NX V2027
  • NX - DRAFTING V2027
  • NX - PMI V2027
Platforms
  • Windows x64 10

KB Article ID# PL8731649

Contents

SummaryDetails

Associated Components