Unable to export a section view to 3D PDF

2023-08-02T01:34:22Z

Summary


Details

After creating a new section view in the assembly navigator, exporting it to Technical Data Package and displaying it in Acrobat Reader, the shape in the section view is not displayed, all shapes are displayed.

Reproduced Steps:

1. Assembly Navigator > select Sections node > New Section...


2. PMI tab > Publish > export 3D PDF


3. Open the exported PDF in a reader such as Acrobat Reader


Solution

The behavior is working as expected.

Workaround:

Please use PMI Section View.

Notes

The only section view supported by Technical Data Package is PMI Section View (PMI tab > Section View). Sections created from the assembly navigator are not supported.

***Please refer to PL8731640 for Japanese article.

Release Versions
  • NX V2212.8100
  • NX - TECH_DATA_PKG V2212.8100
Platforms
  • Windows x64 10

KB Article ID# PL8731643

Contents

SummaryDetails

Associated Components