A fatal error occurs when "//m" is entered in the file name when playing Journal

2023-09-14T01:41:35Z

Summary


Details

When entering "//m" as a file name in the Journal Manager dialog, a memory error occurs and NX terminates.

Reproduced Steps:

1. Start NX > Tools tab > Play

2. Enter “//m” as File Name




Solution

The behavior is due to NX problem and occurs in NX 2007 Series and higher, but the issue is fixed in NX 2312 Series.

Workaround:

Do not enter "//'' + <character string> or "\\'' + <character string> in the file name. (For example, "//a" or "\\m")

Notes

In NX 1980 or lower, the following dialog is output, but the operation can be continued.


***Please refer to PLXXXXXXX for Japanese article.

Release Versions
  • NX V2007
  • NX - SYSENG V2007
Platforms
  • Windows x64 10

KB Article ID# PL8731307

Contents

SummaryDetails

Associated Components