Unable to start Diagramming application

2023-07-31T02:46:53Z

Summary


Details

Even if you select the "Diagramming" creation template in the new creation dialog and perform OK, Diagramming creation environment is not entered and Gateway environment is entered.

Reproduced Steps:

1. File > New > Diagramming tab > select any template > OK


Result:


Solution

The behavior is due to NX problem and has been fixed in NX 2206.4020.

Notes

The problem occurs only in NX 2206 Series.

Note that this only happens if you don't have the NX Diagramming [NX30900] license, i.e. you don't have the "nx_diagramming" feature. The cause is that the algorithm that grabs the token license is not working.

Reference: When it works normally, the "Run Navigator" will open in the resource bar as shown below.


***Please refer to PL8731289 for Japanese article.

Release Versions
  • NX V2206.3000
  • NX - DESIGN V2206.3000
Platforms
  • Windows x64 10

KB Article ID# PL8731292

Contents

SummaryDetails

Associated Components