Unable to change the settings of existing sketches

2023-07-31T02:06:45Z

Summary


Details

Even though changing "Fixed Text Height on Screen" to ON for multiple existing sketches, the change is not reflected. This phenomenon occurs when selecting multiple sketches at a time.

Reproduced Steps:

1. Create multiple sketches with “Fixed Height Text on Screen”=OFF


2. Select multiple sketches in Part Navigator or Graphics > Mouse right click > Settings

3. Set “Fixed Height Text on Screen” to “ON” > OK




Solution

The behavior is working as expected.

In addition, Siemens have received multiple enhancement requests regarding this function.

Notes

Only the first selected existing sketch will be taken into consideration and changed.

Note that not only the "Fix Text Height on Screen" option, but also all other settings in the Sketch Settings dialog, only the first selected sketch is changed.

***Please refer to PL8731281 for Japanese article.

Release Versions
  • NX V2015
  • NX - DESIGN V2015
Platforms
  • Windows x64 10

KB Article ID# PL8731282

Contents

SummaryDetails

Associated Components