NX Zeitstempel passen nicht zusammen

2023-07-27T06:05:37Z
NX for Design

Summary


Details

Time Zone in NX is "GMT" but in windows all settings are "UTC".

Entry in NX syslog:

Not expected and can lead to different Time Stamp in Part History then in Windows Time

*** system log created by seds on Thu Jul 20 10:27:40 2023 GMT

Expected with UTC set in Windows.

*** system log created by huett on Thu Jul 20 13:55:45 2023 W. Europe Daylight Time

Platforms
  • na windows-1064
Release Versions
  • NX V2212.7000
Solution

If there is an Environment Variable TZ=GMT is set before NX start. NX use the value from that Environment Variable as Time Zone.

So in this case may check System Environment and start scripts for the variable "TZ".

Notes

KB Article ID# PL8730363

Contents

SummaryDetails

Associated Components

Modeling