What does the Thin Part to Sheet Metal command do?
SolutionThe Thin Part to Sheet Metal command transforms a uniform thickness solid body to a sheet metal model. In ordered, the command uses a reference face on the input body to identify and marks tabs and bends. In synchronous, it creates native tabs and flanges. The input face defines the thickness for the sheet metal model. You can add sheet metal features to the body as well as edit the thickness or bend radius.