How to Add and Adjust the Alignment of a Custom Symbol to a Note

2024-05-06T14:48:19Z

Summary


Details

How to Add and Adjust the Alignment of a Custom Symbol to a Note

Platforms
  • na windows-1032
Release Versions
  • NX V1980
  • NX V2007
  • NX V2206
  • NX V2212
  • NX V2306
  • NX V2312
Solution

Please see NX video above along with detailed instructions below.

1.  With the Note command launched, place your cursor in the Text Input box where you want the symbol to be inserted and select Custom Symbol from the toolbar.

2.  Locate your Custom Symbol from the Folder View group in the dialog box and select it from the Symbol View window below.

3.  Under the Settings group, select the Vertical Alignment option from the drop-down menu and click OK.  If you do not see the settings group, ensure that your dialog options are set to more in the Dialog Options located in the upper left-hand corner of the dialog.

4.  Now you can enter the text in the Note dialog box and place your note with its accompanying text.

Note:  Below are two alternate methods for aligning the text to your Custom Symbol after the symbol has been added.

1.  With the Note dialog open, right mouse button click on the Custom Symbol, select Alignment, and chose the desired option.

2.  With the Note dialog open, right mouse button click on the Custom Symbol and select Edit.  This will open the Edit Custom Symbol dialog where you can chose the Vertical Alignment from the drop-down menu.  

Notes

KB Article ID# PL8721342

Contents

SummaryDetails

Associated Components