NX JT Files aren't Created when Importing to Teamcenter

2023-07-18T16:02:46Z
NX for Design

Summary


Details

Using the "Import Assembly into Teamcenter" command to import NX files into Teamcenter, the newly created Item Revisions only contain the NX datasets and noJT's a

Solution

If you want to publish the preview file (.qaf) along with the Part file, then while importing the part file, you can switch ON the "Publish Optional Information" option under Import Assembly into Teamcenter Dialog.

Also, if you want to create the JT at the time of import, then you can switch ON the "Publish JT Data".


Notes

Refer to below NX documentation link for reference:
https://docs.sw.siemens.com/en-US/doc/209349590/PL20200605194735749.tcint/xid916862

KB Article ID# PL8721301

Contents

SummaryDetails

Associated Components

Assemblies