Created Planes such as Parallel, Normal to Curve or Tangent appear at the model but not in the PathFinder
2023-07-19T14:46:39Z
Summary
Details
The user creates some Planes such as Parallel, Normal to Curve or Tangent and notices that whilst the resulting planes appear on the model in the graphics window, they are not listed as items in the PathFinder as expected.
A Parallel, a Normal to Curve and a Tangent plane are seen on the model but not in the PathFinder listing
How can they be made visible again in the PathFinder?
Solution
The Planes can be easily made visible again as follows:
Move the mouse cursor over the part name in the PathFinder.
Execute a right-click (Right-Mouse-Button) to open the context menu.
Select 'Ordered PathFinder Display'.
Notice that the 'Planes' option is unexpectedly disabled.