Dialog memory for Measure command not working

2023-07-19T03:16:23Z

Summary


Details

I performed Measure command with the “Create Geometry” option turned on. After that, when I restarted NX and performed the command again, this option was in the OFF state. By Customer Default, "Save Dialog Memory between Sessions" is set to ON, so even in new sessions, the "Create geometry" option should be ON.

Reproduced Steps:

1. Create a box solid > perform the command with “Create Geometry”



2. Restart NX

3. Go to Measure again > Confirm the state


Solution

This behavior was due to NX bug and fixed in NX 2306 Series.

Notes

This behavior occurs in NX 12.0.1 – NX 2212 Series.

In addition to "Create Geometry", the same thing occurs in other options such as "Associative" and "Display Annotation".

***Please refer to PL8721284 for Japanese article.

Release Versions
  • NX V2007
  • NX - DESIGN V2007
Platforms
  • Windows x64 10

KB Article ID# PL8721285

Contents

SummaryDetails

Associated Components