Center of Mass symbol created by Measure moves

2023-07-19T03:15:22Z

Summary


Details

There is a Center of Mass symbol created by Measure command with “Create Geometry” option. Hide and save the Measure feature containing that symbol. When I reopen the part and show the Measure feature, the Center of Mass symbol position changes.

Reproduced Steps:

1. Create a box solid > create a center of Mass symbol by Measure command


2. Hide the Measure feature > save the part


3. Close the part > reopen it

4. Show the Measure feature


Solution

The behavior is due to NX bug and fixed in NX 2312.

For the NX 2306 series, we plan to fix it in NX 2306.3000.

Notes

The issue occurs in NX 1980 - NX 2306.

In addition, it occurs only when the target is a solid body.

***Please refer to PL8721282 for Japanese article.

Release Versions
  • NX V2007
  • NX - DESIGN V2007
Platforms

    KB Article ID# PL8721283

    Contents

    SummaryDetails

    Associated Components