Flattening a face changes its length

2023-07-14T05:00:19Z

Summary


Details

A cylindrical face is flattened using the "Flattening and Forming" command, but it is created with a different length than the source face before flattening.

Reproduced Steps:

1. After creating a cylinder, divide the face at the position you want to flatten


2. Flattening and forming command > select the face to flatten


3. Compare the source face edge and flattened face edge length


Solution

The behavior is working as expected.

Notes

"Flattening and Forming" command does not use the tolerance value defined in the “Modeling Preferences", it uses a fixed value "0.001" set inside the command.

***Please refer to PL8721213 for Japanese article.

Release Versions
  • NX V2212.5000
  • NX - DESIGN V2212.5000
Platforms
  • Windows x64 10

KB Article ID# PL8721214

Contents

SummaryDetails

Associated Components