Can I have multiple draft analysis results?

2023-07-12T03:17:21Z

Summary


Details

After performing the first draft analysis, I performed a new draft analysis again and selected a model, but the existing draft analysis was selected. Does this behavior mean that I can't have multiple results?

Reproduced Steps:

1. Analysis tab > Draft Analysis (in Face Shape Group)


2. After again repeat the step 1 above, expand Draft Analysis in Part Navigator

** There is only one Draft Analysis.


Solution

The behavior is working as expected.

This is due to an existing Draft Analysis (Feature) was selected when specifying the target faces.

Workaround:

When performing the command, set “Face" in “Type Filter" or exclusion of “Analysis" by “General Selection Filters" > “Detailed Filtering...".


Notes

***Please refer to PL8721187 for Japanese article.

Release Versions
  • NX V1953
  • NX - STUDIO_DESIGN V1953
Platforms
  • Windows x64 10

KB Article ID# PL8721188

Contents

SummaryDetails

Associated Components