Solids cannot be selected with "Move to Layer"

2023-07-12T02:18:55Z

Summary


Details

There are multiple solids in one component, and when I perform "Move to Layer" to change the layer of one solid, the solid cannot be selected and the entire component is selected.

Reproduced Steps:

1. Create an assembly, a subassembly and some solids

2. Go to View tab > Layer to Move > select a solid body


Solution

This behavior is working as designed.

The cause is that the setting of “File > Preferences > Assembly > Component > Selection > Component Member Select” is to OFF. The solid can be selected by setting it ON.

Workaround:

If you want to select a solid while the setting is OFF, please do one of the following.

1. Perform the command after selecting solid body

2. Perform the command after excluding "Component" in "General Selection Filter" > "Advanced Filter..." > "Type"

3. After performing the command, filter to "Solid Body" with "Type Filter"


Notes

All commands that use the Class Selection dialog box, such as Edit Object Display, will behave in the same way.

***Please refer to PL8721185 for Japanese article.

Release Versions
  • NX V12.0.2
  • NX - GATEWAY V12.0.2
  • NX - ASSEMBLIES V12.0.2
  • NX - DESIGN V12.0.2
Platforms
  • Windows x64 10

KB Article ID# PL8721186

Contents

SummaryDetails

Associated Components