Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix controllers for "7R_AXIS_INVERSE, ABB_RAPID, ABB_RAPID_VOLVO, CLOOS_CAROLA, CLS_UPLOAD, COMAU_PDL, COMAU_PDL_VOLVO, DEFAULT, DENSO_PACSCRIPT, DUERR_ECOTALK, EPSON_SPEL, FANUC_F100, FANUC_RJ, FANUC_RJ_JAPAN, FANUC_RJ_VW, FANUC_RRS_INVERSE, HHI_HRBASIC, IGM_INS, KAWASAKI_AS, KAWASAKI_CKE, KUKA_KRC, KUKA_KRC_BMW, KUKA_KRC_VOLVO, KUKA_VKRC, MITSUBISHI_MELFA, NACHI_SLIM, NC_CODE, NC_CODE_BMW, NC_CODE_EMBRAER, NC_CODE_RIVETING, OLP_FUNC, OLP_TOOL, PANASONIC_CSR, REIS_ROBSTAR, ROBOTIC_PARAMETERS_VIEWER, ROLLER_HEMMING_TOOL, SEGMENTIZER, STAUBLI_VAL, TCP_TRAVEL_DISTANCE_FUNC, TRALLFA_ROBTALK, UNIVERSAL_URSCRIPT, UPLOAD_ROBCAD_ROBOTIC_PROGRAM, XACT_DUAL_ARM, YASKAWA_INFORM"
are available for download from https://support.sw.siemens.com.
See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'OLP Change Logs' folder directly under the 'Process Simulate Robot Controllers' folder.
Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'Process Simulate Robot Controllers'
- Select 2307
Download the file(s):
Tecnomatix_2307_7R_AXIS_INVERSE_64BIT_v1.2_07_02_2023.exe
Tecnomatix_2307_ABB_RAPID_64BIT_v5.19_06_07_2023.exe
Tecnomatix_2307_ABB_RAPID_VOLVO_64BIT_v5.9.4_31_03_2023.exe
Tecnomatix_2307_CLOOS_CAROLA_64BIT_v2.34_31_03_2023.exe
Tecnomatix_2307_CLS_UPLOAD_64BIT_v1.13.2_06_07_2023.exe
Tecnomatix_2307_COMAU_PDL_64BIT_v5.5.8_03_04_2023.exe
Tecnomatix_2307_COMAU_PDL_VOLVO_64BIT_v2.14.7_31_03_2023.exe
Tecnomatix_2307_DEFAULT_64BIT_v2.119_07_06_2023.exe
Tecnomatix_2307_DENSO_PACSCRIPT_64BIT_v2.37_31_03_2023.exe
Tecnomatix_2307_DUERR_ECOTALK_64BIT_v2.80_31_03_2023.exe
Tecnomatix_2307_EPSON_SPEL_64BIT_v2.27_31_03_2023.exe
Tecnomatix_2307_FANUC_F100_64BIT_v2.37_31_03_2023.exe
Tecnomatix_2307_FANUC_RJ_64BIT_v3.88.1_16_06_2023.exe
Tecnomatix_2307_FANUC_RJ_JAPAN_64BIT_v2.161.1_16_06_2023.exe
Tecnomatix_2307_FANUC_RJ_VW_64BIT_v3.22.2_22_06_2023.exe
Tecnomatix_2307_FANUC_RRS_INVERSE_64BIT_v1.2.1_13_04_2023.exe
Tecnomatix_2307_HHI_HRBASIC_64BIT_v1.14_31_03_2023.exe
Tecnomatix_2307_IGM_INS_64BIT_v1.54_31_03_2023.exe
Tecnomatix_2307_KAWASAKI_AS_64BIT_v5.28_06_07_2023.exe
Tecnomatix_2307_KAWASAKI_CKE_64BIT_v1.20_06_07_2023.exe
Tecnomatix_2307_KUKA_KRC_64BIT_v6.6_06_07_2023.exe
Tecnomatix_2307_KUKA_KRC_BMW_64BIT_v4.23_06_07_2023.exe
Tecnomatix_2307_KUKA_KRC_VOLVO_64BIT_v2.29.8_31_03_2023.exe
Tecnomatix_2307_KUKA_VKRC_64BIT_v7.9_16_06_2023.exe
Tecnomatix_2307_MITSUBISHI_MELFA_64BIT_v0.29_31_03_2023.exe
Tecnomatix_2307_NACHI_SLIM_64BIT_v5.6.1_23_06_2023.exe
Tecnomatix_2307_NC_CODE_64BIT_v2.12_22_06_2023.exe
Tecnomatix_2307_NC_CODE_BMW_64BIT_v1.18.7_31_03_2023.exe
Tecnomatix_2307_NC_CODE_EMBRAER_64BIT_v1.15.7_31_03_2023.exe
Tecnomatix_2307_NC_CODE_RIVETING_64BIT_v1.13.7_31_03_2023.exe
Tecnomatix_2307_OLP_FUNC_64BIT_v1.0.4_08_02_2023.exe
Tecnomatix_2307_OLP_TOOL_64BIT_v15.15.3_31_05_2023.exe
Tecnomatix_2307_PANASONIC_CSR_64BIT_v2.31_31_03_2023.exe
Tecnomatix_2307_REIS_ROBSTAR_64BIT_v2.45_31_03_2023.exe
Tecnomatix_2307_ROBOTIC_PARAMETERS_VIEWER_64BIT_v1.1.4_31_05_2023.exe
Tecnomatix_2307_ROLLER_HEMMING_TOOL_64BIT_v1.0.10_07_06_2023.exe
Tecnomatix_2307_SEGMENTIZER_64BIT_v3.2_24_01_2023.exe
Tecnomatix_2307_STAUBLI_VAL_64BIT_v4.15_06_07_2023.exe
Tecnomatix_2307_TCP_TRAVEL_DISTANCE_FUNC_64BIT_v1.1.5_23_05_2023.exe
Tecnomatix_2307_TRALLFA_ROBTALK_64BIT_v1.60_23_05_2023.exe
Tecnomatix_2307_UNIVERSAL_URSCRIPT_64BIT_v6.35_31_03_2023.exe
Tecnomatix_2307_UPLOAD_ROBCAD_ROBOTIC_PROGRAM_64BIT_v2.8_16_11_2022.exe
Tecnomatix_2307_XACT_DUAL_ARM_64BIT_v1.36_31_03_2023.exe
Tecnomatix_2307_YASKAWA_INFORM_64BIT_v6.45_06_07_2023.exe
To Install:
Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software