Solid Edge Cannot apply centrelines to pattern of slots

2023-07-07T12:35:23Z
DRAFT

Summary


Details

 The customer has a part with a slot feature from which they have created a pattern.


When they create a drawing from the part and apply 'Automatic Centerlines', these are not applied to the pattern - only to the slot feature.


Solution

Effectively, there is only a single profile and slot ID for the slot feature itself. Currently, the software only supports a unique slot ID and its respective slot profile for subsequently creating a centerline/center mark.  This is why the centerlines are only applied to the original slot.

KB Article ID# PL8721135

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS