About specifying "2D Section Library" and "Feature Template Library" Custome Defaults to the same folder

2023-07-04T07:40:17Z

Summary


Details

Steps to reproduce the issue:

1. Create a sample folder for e.g. test to "C:\".

2. Start NX.

3. File -> Utilities -> Customer Defaults.

4. Gateway -> Reuse Library -> Modeling -> 2D Section Library.

Set the setting as below.

CAD-2D Library|C:\test

5. Gateway -> Reuse Library -> Modeling -> Feature Template Library.

Set the setting as below.

CAD-3D Library|C:\test

6. [OK] the Customer Defaults dialog.

7. Restart NX.

8. Create a new part file using Blank template.

9. Display "Reuse Library" from resource bar

-> only "CAD-2D Library" is displayed, "CAD-3D Library" is not displayed.

Solution

When the library path is the same, only one of them can be displayed, this is designed as intended. It is suggested that the paths of the two libraries be different.

KB Article ID# PL8721088

Contents

SummaryDetails

Associated Components