If VR is executed with the data, then are there any differences with the data stored in Tc and standalone NX?
Can the data be made to operate in the same way as standalone NX VR?
SolutionOnce the model is transferred to NX VR (either from native or managed NX), they operate the same way. There will be some differences in model/part/assembly names internally but functionality wise, everything should be the same.