How to modify line width for custom symbol when export PDF

2023-10-02T16:42:26Z

Summary


Details

After exporting pdf of custom symbol, sometimes the line width does not have the same thickness as it is in NX, why? 

Platforms
  • INTL64 windows-764
Release Versions
  • NX V12.0.2
Solution

To verify the real line width of a custom symbol, you would need to smash the symbol and then you can modify it.

1)    Select the symbol ->RM ->Smash

2)    Information -> Object -> select the curves -> you would see:


.70 was the original width before view dependently edited, so you can edit the width as below:

 Select the sheet from PNT -> RM -> View Dependent Edit -> Add Edits -> Edit Entire Object-> Set Line width to .13 -> Apply -> Rectangle select -> OK

Alternatively, you can also turn off "Show Width" from Preferences, Visualization -> Color/Font ->Drawing and Layout Part Settings if you wish not to display objects' widths, and without smashing the custom symbol.

Notes

KB Article ID# PL8721077

Contents

SummaryDetails

Associated Components