An NX part file (*.prt) cannot be opened via the File Explorer in Solid Edge CAM Pro.

2023-07-07T13:39:47Z

Summary


Details

A user tries to open an NX part file (*.prt) in Solid Edge CAM Pro via the File Explorer by right mouse clicking on the file and selecting the 'Open' command in the context menu of the selected file.

'Open' command in the context menu of the selected NX part file

Whilst the Solid Edge CAM Pro session will be started, it appears the NX part file is not opened as expected.

started Solid Edge CAM Pro session without an opened NX part file

Solution

The situation can be resolved by checking and correcting the default app for the file type .prt (PRT File) via the following steps on the operating system:

  • Select the 'Windows Start' icon and choose 'Settings'
    Windows Start > Settings

    • Select the 'Apps' group
      Windows Settings > Apps

      • Select 'Default apps'
        Default apps

        • Select 'Choose default apps by file type' in the 'Default apps' area
          Choose default apps by file type

          • Scroll to the file type .prt (PRT File)
            • Notice the chosen default app (in case of the user it is set to NX)
              default app NX for the file type .prt (PRT File)

              • Click on the defined default app
                • Redefine the default app by selecting 'Siemens Industry Software Inc. Component'
                  redefining the default app with 'Siemens Industry Software Inc. Component'

                  • Close the 'Settings' dialog with the redefined default app
                    'Settings' dialog with the redefined default app

                    • Double-click respectively open the NX part file via the File Explorer
                      • The NX part file will now be opened in Solid Edge CAM Pro as expected
                        opened NX part file in Solid Edge CAM Pro

                        KB Article ID# PL8721069

                        Contents

                        SummaryDetails

                        Associated Components