Bridge Curve in NX2306 can now select Curves

2024-03-07T16:09:29Z

Summary


Details

 Prior to NX 2306, the Bridge Surface function would only select edges.

Solution

 New in NX2306 is the ability to select curves as well as edges. See the above video for the procedure.

Bridge Curve in NX2306 Can Now Select Curves

1.       Open the part file.

2.       Choose the Surface tab -> Base group -> More -> Bridge Surface.

3.       In the Bridge Surface dialog, above the Select Edge options, Edge or Curve can now be selected.

-          Note: This feature became available in NX 2306.

KB Article ID# PL8721039

Contents

SummaryDetails

Associated Components