How to create the table for the Track Drawing Changes.

2023-07-04T06:25:20Z

Summary


Details

The user needs to add a table similar to the report to the drafting sheet (like a hole table or part list). instead of a separate report.

Solution

We can add having results in the tabular note by copy/paste.

1. Export a Detailed Results list into the spreadsheet.


2. Create a tabular Note in NX.

3. Select a tabular Note, right-click choose Edit Using Spreadsheet.


4. Copy/Paste  Detailed Results  spreadsheet text in the tabular note spreadsheet.[Note: there is no link between the results and the tabular note].

5. Once it copy-pastes the results, select a tabular note, right-click, and choose "Edit Without Spreadsheet".

6. In the Edit Tabular Note Without Spreadsheet Warning message, click OK.

Note: Edit Tabular Note Without Spreadsheet option is reduce your time to update tabular notes.

Notes

IR#10750516

KB Article ID# PL8721034

Contents

SummaryDetails

Associated Components