NX How to use the utility tcin_template_setup.bat using -s option?

2023-07-04T02:52:07Z
NX System Administration NX for Design

Summary


Details

How to use the utility tcin_template_setup.bat using -s option?

Solution

The “-s” this option will be used to skip importing templates from the specified directory under the NX install folder.

e.g. You can specify the “simulation” in the file, and provide its path to the “-s=” switch, then the simulation templates will get skipped.

If you want to only install the specific Templates and skip the other templates like Drafting and Modelling, then create a text file like 'drafting1.txt' and add the Title of all the folders where Template files reside. Like, Drafting, UGII, MACH, Routing, etc., and use the below syntax while import

tcin_template_setup.bat -u=infodba -p=infodba -s=C:\1451\drafting1.txt

See the below snap-


Notes

KB Article ID# PL8720993

Contents

SummaryDetails

Associated Components

Installation