A method to specify default refset when adding components

2023-07-05T16:30:15Z

Summary


Details

Can users specify the default reference set when adding components?

Platforms
  • INTL64 windows-1064
Release Versions
  • NX V1996
Solution

1) Users can create a non-standard user Reference set in the customer defaults under File-> Utilities-> Customer Defaults-> Assemblies-> Site Standards-> Reference Sets-> User Reference Sets-> Additional Model Reference Sets.

Below we specify MyRefSet1 as such a reference Set


2) Users can define a dialog Favorite in the Add Component dialog to use the Reference Set specified in the customer default set above.


For more information on creating and saving dialog favorites please see the NX documentation at

https://docs.sw.siemens.com/en-US/doc/209349590/PL20221117716122093.nx_interface/id1356126

Notes

KB Article ID# PL8720954

Contents

SummaryDetails

Associated Components