NX Using Export or Import STEP 214 to preserve assembly structure with component bodies

2023-07-03T12:32:01Z
NX for Design

Summary


Details

Using Export or Import STEP 214 to preserve assembly structure with component bodies

Solution

For the export STEP 214, the Entire Part option must be selected to preserve the assembly structure.  The STEP file can then be imported into a file without the Flatten Assembly option checked, or the STEP file can be opened which will also preserve the assembly structure.



KB Article ID# PL8720943

Contents

SummaryDetails

Associated Components

CAD Translators