ERROR 1525 when using utility ugtopv.exe

2023-09-18T10:06:41Z

Summary


Details

In some cases the utility ugtopv.exe returns an error:

ERROR 1525 :Teamcenter Error:Failed to import into Teamcenter item [%UGMGR=V3.2 PH=R1DAAAfhJSJkjB PRH=hlAAAAfhJSJkjB PN=000691 PRN=A RT="has shape" AT="UG master part file" ] the file [RcCAAEg3JSJkjB.jt] RefSetName [TopOfAssembly]

The NX syslog reports the following FMS error:

Unrecognized FMS error -211 was encountered

Platforms
  • na windows-1064
Release Versions
  • NX V2212
  • NX V2306
Solution

The error could be avoided by updating the setting OutputDirectory from "./" to "" in the applicable config file:

OutputDirectory = ""

Please note that the applicable config file is specified using the -config argument or the default one that comes with the NX installation (%UGII_BASE_DIR\pvtrans\tessUG.config).

Notes

KB Article ID# PL8720815

Contents

SummaryDetails

Associated Components