NX Set Flat Solid preference "fix at time-stamp" to unchecked by default

2023-09-12T13:42:41Z
NX for Design

Summary


Details

In NX12

Is there a Customer Default to control Flat Solid setting "fix at time-stamp" to unchecked? In NX12 Flat Solid command has “Fix at Current Timestamp” unchecked.

In NX2206, this setting is on by default.


Platforms
  • na windows-1064
Release Versions
  • NX V2206
Solution

Yes, there is a customer default for "Fix at Timestamp" for Flat Solid feature in both Sheet Metal and FPCD application. The Location of this customer default settings is shown in below image.



Note: This customer default available under Flat Pattern Treatments is applicable for both Flat Pattern and Flat Solid.

 This setting is currently only PART scope, not session scope.

With Part Scope customer defaults, you would need to open the Model Template part and toggle off "Fix at current Timestamp", then newly parts created using Model Template will have this setting toggled off.

According to the NX doc:

Part Scope: applies only to subsequently created parts. (When you are using seed or template parts in Teamcenter Integration, part settings that are already stored in the seed or template parts are not affected.)

Notes

KB Article ID# PL8720726

Contents

SummaryDetails

Associated Components

Sheet Metal