In this scenario, the user finds that in Solid Edge Simulation, version 2023 Update 5 , the setting 'Contour style' as "ISO-Contour" does not create a plot result for the ISO contour style.
- Open a part and calculate the simulation.
- In the calculation result, select 'Contour style' as "ISO-Contour".
Problem: No Contour Plot is displayed.
Deselect the setting "Generate only Surface results" and the Iso Contour Plot will be displayed.
With the setting "Generate only Surface results" nothing is displayed.
Notes