Error - A datum referenced in this FCF is not defined in the current part context

2023-06-14T07:33:20Z

Summary


Details

I ran Advisor Check to validate PMI and it shows an error even though the datum is existed.

Reproduced Steps:

1. Create a model including Feature Control Frame and Datum Target

2. HD3D Tool > PMI Advisor > Run Advisor Check


Solution

The behavior is working as expected.

PMI Advisor command checks Datum Feature referenced by Feature Control Frame, but Datum Target is outside the scope of checking due to not supported as the reference.

In addition, Datum Target is added as processing target in NX 2212 Series.


WORKAROUND:

Define Datum Feature Symbol (Instead of Datum Target)

Notes

***Please refer to ***Please refer to PL8720689 for Japanese article.

Release Versions
  • NX V2206
  • NX - MBD V2206
Platforms
  • Windows x64 10

KB Article ID# PL8720690

Contents

SummaryDetails

Associated Components