In NX Classic theme, the toggle button ON/OFF in the pull-down list cannot be judged.

2023-06-14T07:30:42Z

Summary


Details

If you set "Classic" as NX Theme in User Interface Preferences, e.g, you cannot find whether the toggle state of each command displayed in the pull-down list in Sketch environment is ON or OFF.

Reproduced Steps:

1. File > Preferences > Visualization > Thema > NX Thema > Classic

2. In Sketch environment >Solve group> Options

*** The display status cannot be found even if the toggle such as "Display Persistent Relations" is turned ON. (Compare with "Light (Recommended)" below)


***Below is a comparison of the "Display Auto Dimensions" pull-down under the old sketch environment.


WORKAROUND:

Please use NX Thema other than “Classic”

Solution

The behavior is due to NX problem and is fixed in NX 2306 Series.


Notes

The behavior occurs in NX 1980 – NX 2212.

In addition, the problem occurs only in “Classic”, does not occur in other theme such as Light((Recommends), “Light Gray” and “Dark”.

***Please refer to PL8720687 for Japanese article.

Release Versions
  • NX V2212
  • NX - SYSENG V2212
Platforms
  • Windows x64 10

KB Article ID# PL8720688

Contents

SummaryDetails

Associated Components