Copying/Pasting a component with the special character "(" or ")" in its name will automatically convert it to "_"

2023-06-14T07:21:47Z

Summary


Details

When checking a component name after "Copy/Paste" it, the name of the source component is not inherited and the strings "(" and ")" are replaced with "_". Is this behavior as designed by NX?

Reproduced Steps:

1. Select a component in Assembly Navigator > Mouse right click > select Properties


2. General tab > Name. Change the name of the component, e.g, from “MODEL1” to “MODEL1(test)”

3. Select Apply Name to All Occurrences > OK



4. Copy/Paste the component

5. Perform “Unpack" if component is packed

*** "(" and ")" strings are converted to "_".


Solution

The behavior is working as expected. The special characters “(“, “)” or others which is allowed to use will be converted to “_” automatically after “Copy/Paste”. If you don't want this behavior, Siemens recommend you don't use special characters.

WORKAROUND:

Please change the component name manually after pasting.

Notes

This behavior is the same when creating new components as well.


***Please refer to PL8720685 for Japanese article.

Release Versions
  • NX V11.0.2
  • NX - ASSEMBLIES V11.0.2
Platforms
  • Windows x64 10

KB Article ID# PL8720686

Contents

SummaryDetails

Associated Components