How to Create a PMI Perimeter Dimension

2023-06-19T11:36:38Z

Summary


Details

How to Create a PMI Perimeter Dimension

Solution

 1. In an existing sketch, create a Perimeter dimension.

2.  Exit the sketch and in PMI, select 'Note', then the Expressions icon in the ribbon.


In the Expressions dialog, select the Perimeter expression -OK.


Back in the PMI Note dialog, enter additional text as needed "Perimeter=" and place the dimension where needed. 

 Note: This is associative. If the Perimeter expression is edited this note will update.


KB Article ID# PL8720677

Contents

SummaryDetails

Associated Components