How to Add a Palette of Tables to the Resource Bar

2024-03-07T16:03:36Z

Summary


Details

How to create a Palette of Tables and add them to the Resource Bar.

Solution

See the above video for the procedure that shows how to add a tab to the Resource Bar that has additional palettes.

How to Add a Palette of Tables to the Resource Bar

1.       Open the Drawing.

2.       In the Top Border Bar, choose Menu -> Preferences -> Palettes.

3.       In the Palette dialog, click Palette.

4.       In the Open Palette dialog, click Browse.

5.       Select the Pax file, tables.pax.

-          Note: The file path is as follows: This PC > System (C:) > Program Files > Siemens > NX2212 > UGII > table_files. The NX folder will change based on the NX version.

6.       Click OK.

7.       Click OK.

8.       A new palette of tables will appear in the Resource Bar.

9.       Click on the desired table.

10.   Click in the Display to place.

KB Article ID# PL8720619

Contents

SummaryDetails

Associated Components