Unable to align Datum Feature Symbol to Feature Control Frame

2023-06-08T02:18:25Z

Summary


Details

There is a Feature Control Frame that is stacked on a PMI Radial dimension. I am unable to align and place a Datum Feature Symbol with a leader line to that Feature Control Frame. Note that if the Feature Control Frame is not stacked with the PMI Radial dimension, it can be placed.

Reproduced Steps:

1. Create a PMI Radial dimension and a Feature Control Frame


2. Create a Datum Feature Symbol with a leader line aligned to the Feature Control Frame

As shown in the picture below, unable to create it with the leader line.( However, able to create without the leader.)


If Feature Control Frame exists independently, it can be created as follows.


Solution

This behavior is working as expected. Datum feature Symbol cannot be directly aligned with a leader line to a Feature Control Frame that is stacked.

WORKAROUND:

Create by aligning with the PMI Radial dimension that is the parent of the Feature Control Frame


or

Create Datum Feature Symbol without the leader line

Notes

***Please refer to PL8720594 for Japanese article.

Release Versions
  • NX V1926
  • NX - PMI V1926
Platforms

    KB Article ID# PL8720595

    Contents

    SummaryDetails

    Associated Components