Earliest version of Solid Edge supported on Windows 11

2023-05-30T15:43:40Z

Summary


Details

What is the earliest version of Solid Edge supported on Windows 11?

Solution

Solid Edge 2022 MP2 is the earliest version of Solid Edge supported on Windows 11.

From the SE2022 MP2 readme file:

https://support.sw.siemens.com/en-US/downloads/PL20200902110958364/akamai?uri=https%3A%2F%2Fdownloada.industrysoftware.automation.siemens.com%2Fsc_downloads_prod%2Ff%2F7%2Fc7ff1f6f12b94bd4944579666ba02207%2FSolid_Edge_2022_MP2_Readme.txt


Notes

KB Article ID# PL8719837

Contents

SummaryDetails

Associated Components